Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

STEP importing into wireframe

Pioneer
Pioneer

Hi everyone, my issue today is that I am importing a STEP file into SE (choosing assembly as template) and it works, but the parts imported are shown as a wireframe. Even when the shaded with edges option is chosen, cause I never touched that. You can see it in the picture. 

 

image.png

 

Is there some reason why this happens? Any way to fix it? Thanks. 

===================================================

ST9 and Ordered environment.
5 REPLIES 5

Re: STEP importing into wireframe

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I'm not certain what's going on. Maybe someone else knows. In the meantime if you could upload just one of the parts, not the assembly, but a small part which is in the assembly, that might give a clue.

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Re: STEP importing into wireframe

Pioneer
Pioneer

Sure, done. I attached a small part in the first post. 

===================================================

ST9 and Ordered environment.

Re: STEP importing into wireframe

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

The parts have no color. Use part painter to add color to the parts.

edit: by the way, they also have no assigned material which means your templates also do not. So assigning a material will also add color.

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Re: STEP importing into wireframe

Pioneer
Pioneer

@bshand wrote:

The parts have no color. Use part painter to add color to the parts.


LOL. You have to be kidding me! It worked... Smiley LOL 

 

Yeah well, you can see where I'm coming from. First week with SE. 

 

Thanks...

===================================================

ST9 and Ordered environment.

Re: STEP importing into wireframe

Gears Phenom Gears Phenom
Gears Phenom

@-Axel-   don't feel bad,  I've ran SE for almost 20 years now and I would never have thought of that!!!

 

Way to go @bshand

Matt Johnson
Solid Edge Certified Professional
Solid Edge 2019 (SEEC) - Production
NX12 (Tc Integration)
Teamcenter 10.1.7