Cancel
Showing results for 
Search instead for 
Did you mean: 

Save / Export / Import Custom Settings

Experimenter
Experimenter

Looking for a way to save Solid Edge ST8 settings so they can be exported/imported to other computers.  Is there a quick and "clean" way to do this?

2 REPLIES 2

Re: Save / Export / Import Custom Settings

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

When you save your import/export options, you are asked to save an INI file to another location.  Place that modified INI file on a network share and ask everyone to specify it when they use a translator.  It will remain the default after the initial change to the new INI.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com