Cancel
Showing results for 
Search instead for 
Did you mean: 

Save as 3d PDF

Pioneer
Pioneer

Hello,

 

I have a bit of my macro which saves a pdf, but now i want to export the asm or par as 3d pdf, can you guys point me in the right direction and/or help me a bit?

 

This is the code to save my draft as pdf, which isn't neccesary anymore, because we use an add-in which exports a pdf every time i save the document.

 

And i know i have to change some more things, because it was used to be for the draft environment.

 

Private Sub Button_SaveAsPDF_Click(sender As Object, e As EventArgs) Handles Button_SaveAsPDF.Click

        Form1.SEDraftDocument = Main.seApp.ActiveDocument

        'Het pad specificeren waar het bestand moet worden opgeslagen
        Dim SESaveAsPDFPath As String
        SESaveAsPDFPath = TextBox_OpslaanIn.Text & "\" & TextBox_Bestandsnaam.Text & ".pdf"

        'Extra check zodra bestandsnaam wordt gewijzigd --> infobox 
        If TextBox_Bestandsnaam.Modified = True Then
            Select Case MsgBox("Weet je zeker dat je de bestandsnaam wilt wijzigen?", MsgBoxStyle.YesNo, Title:="Bestandsnaam gewijzigd")
                Case MsgBoxResult.Yes
                    Form1.SEDraftDocument.SaveAs(SESaveAsPDFPath)
                    Me.Close()
                Case MsgBoxResult.No
                    Main.SEDocumentPropertySets = SEModelDocument.Properties

                    'Vul bij bestandsnaam de document number van het gelinkte model + de bestandsnaam zonder extensie
                    For i As Integer = 1 To Main.SEDocumentPropertySets.Count
                        Main.SEDocumentProperties = Main.SEDocumentPropertySets.Item(i)
                        For j As Integer = 1 To Main.SEDocumentProperties.Count
                            Main.SEDocumentProperty = Main.SEDocumentProperties.Item(j)

                            If Main.SEDocumentProperty.Name = "Document Number" Then
                                TextBox_Bestandsnaam.Text = Main.SEDocumentProperty.Value & " " & SEDocumentName(0)
                            End If
                        Next
                    Next
            End Select
        Else
            Form1.SEDraftDocument.SaveAs(SESaveAsPDFPath)
            Me.Close()
            SESheetWindow.Update()
        End If

        'Check of de draft al is opgeslagen
        If Form1.SEDraftDocument.Path = "" Then
            Select Case MsgBox("Het draft document is nog niet opgeslagen. Wilt u deze nu opslaan?", MsgBoxStyle.YesNo, Title:="Draft niet opgeslagen")
                Case MsgBoxResult.Yes
                    Form_SaveAs.Show()
                    Me.Close()
            End Select
        End If

    End Sub

Thanks folks!

4 REPLIES 4

Betreff: Save as 3d PDF

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @JuRi

 

 

 

try to modify the save line for the PDF with ...(SEPDFPath, ,True)

 

This additional parameter (which IMHO is not described in any documentation) gives a 3D PDF as output format, rather than a 2D PDF

 

 

regards
Wolfgang

Betreff: Save as 3d PDF

Pioneer
Pioneer

This seems to return just the normal pdf for me. I've put some thing of the code underneath. my SESaveAsPDFPath returns ............................\filename.pdf

 

    Public SEPartDocument As SolidEdgePart.PartDocument
    SEPartDocument = Main.seApp.ActiveDocument
    Dim SEPartDocumentpath() As String

SEPartDocument.SaveAs(SESaveAsPDFPath, True)

 

 

Betreff: Save as 3d PDF

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @JuRi

 

 

 

 

double commas!

 

 

 

SEPartDocument.SaveAs(SESaveAsPDFPath, ,True)



JuRi schrieb:

This seems to return just the normal pdf for me. I've put some thing of the code underneath. my SESaveAsPDFPath returns ............................\filename.pdf

 

    Public SEPartDocument As SolidEdgePart.PartDocument
    SEPartDocument = Main.seApp.ActiveDocument
    Dim SEPartDocumentpath() As String

SEPartDocument.SaveAs(SESaveAsPDFPath, True)

 

 


 

regards
Wolfgang
Highlighted

Betreff: Save as 3d PDF

Pioneer
Pioneer

Thanks! This did the trick.