Cancel
Showing results for 
Search instead for 
Did you mean: 

Save as ACAD result in SE crash

Dear SE users,

we have some problems with translating draft drawings into DWG and DXF format. Allmost every translation it crashes.

I have cross checked every setting in the SEACAD.ini and settings of the SEACAD.ini location.

For some reason it was changed into the roaming location in the user location...

 

The problem started with MP4 for ST7.

 

Are there users that have the same problem?

-------
Daniël Schuiling
Solid Edge ST7
Teamcenter 10
12 REPLIES

Re: Save as ACAD result in SE crash

Phenom
Phenom

Sorry but I haven't seen this issue. However I only save to DFX with version 2007. So you may want to try opening options when saving and see which release you're saving to.

 

Bob

 

 

Re: Save as ACAD result in SE crash

Hi Bob,

thank you for the reply.

 

We have tried to save it as DXF and DWG, versions 2000 and 2007. All crash.

It is not only me but all my colleagues have the same problem.

 

Is it possible that you could send me your SEACAD settings?

-------
Daniël Schuiling
Solid Edge ST7
Teamcenter 10

Re: Save as ACAD result in SE crash

Phenom
Phenom

Daniel

 

Here you go.

 

Bob

Re: Save as ACAD result in SE crash

Genius
Genius

I've had this problem with a previous version. It wouldn't do PDF's either! The solution was we completely uninstalled SE and reinstalled it. I guess something went wrong in the first install.

 

Not a first choice, but if all else fails....

Re: Save as ACAD result in SE crash

Hmm, I don't like that.
That means that every SE installation in our company went wrong. I find it hard to believe.
-------
Daniël Schuiling
Solid Edge ST7
Teamcenter 10

Re: Save as ACAD result in SE crash

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

If the case has worsened to the extent that a re-installation seems to be the last resort, repairing the Solid Edge part of registry can probably get it working.

In case you decide to, reset the HKEY_CURRENT_USER Solid Edge registry:

HKEY_CURRENT_USER\Software\Unigraphics Solutions\Solid Edge

Simple delete this and restart SE

Not sure if any DWG export settings are stored in the registry, this is just a guess.

 

Re: Save as ACAD result in SE crash

Already tried that. No result.
I will try to reinstall SE, not happy about this but I will give it a try.
-------
Daniël Schuiling
Solid Edge ST7
Teamcenter 10

Re: Save as ACAD result in SE crash

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

You could try enabling logging on the options dialog before you Save As.

The log may contain a clue.

LMGi
www.TLMGi.com

Re: Save as ACAD result in SE crash

Just had the support on the phone.
There is a possibility that there is a network problem.

I have asked if the IT could add the SE extensions so this don't get scanned. When the problem still happens I'm going to work local.

Hope it gives some answers.

I thank you all for the given answers, perhaps I will solve this problem.
-------
Daniël Schuiling
Solid Edge ST7
Teamcenter 10