Cancel
Showing results for 
Search instead for 
Did you mean: 

Save as image

Pioneer
Pioneer

I have found some where (but now forgotten) that explain how to "export" model image to excel or any other microsoft package without any pixel distortion on stretching. 

 

I have tried save as image and paste it to excel but its pixels distorted on stretching.

 

kindly suggest

5 REPLIES 5

Re: Save as image

Legend
Legend

Hi, you can copy a draft view and paste it straight into excel. Is that what you meant?

Highlighted

Re: Save as image

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Place a drawing view of the model in Draft (use a saved view if you want a non-standard orientation).

Shade the drawing view to look just as in the model.

Copy the drawing view from Draft and then paste directly in Word/Excel.

This will not distort.

  

~Tushar

 

Re: Save as image

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @AM2,

 

Further to what others have suggested......you might check the "Options" for the image file format [Type] selected, and make some increased [size & quality] settings there, if you haven't already.

 

SE_DFT_SaveAsImage_Options.png

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP7] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Save as image

Pioneer
Pioneer

Yes this is what I was looking for. But it is not reflecting shadded model. (colored) when I paste it in excel. It pastes in the form of Wire Frame.
What could be the problem? 

Re: Save as image

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Strangely enough Smiley Frustrated a shaded view from SE Draft pastes shaded in Word but wireframe in Excel (and PowerPoint and Wordpad and MS Paint - for the record).

    

As a workaround, paste first in Word (or a Outlook message) as shaded, then copy shaded from Word (or Outlook) again and paste in Excel

  

So what's common in Word and Outlook that is missing in Excel, Wordpad and MS Paint - Spellchecker ? Robot LOL

   

~Tushar