Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Save draft file to desktop from Teamcenter

Valued Contributor
Valued Contributor

I dont know if this can be done. My company uses Solid Edge with Teamcenter. If solid edge is connected to teamcenter, files are opened thru the server and teamcenter manages the file. If solid edge is not connceted to teamcenter files are opened from the PC disk drive. What I want to do, is to save a file I have opened from teamcenter to my local hard drive. I cannot see a way to do this either in Solid edge or in teamcenter.

3 REPLIES

Re: Save draft file to desktop from Teamcenter

Esteemed Contributor
Esteemed Contributor

I don't have TC but I have used it and somewhere there is a "create unmanaged copy" function. Maybe not those words, which are from Insight, but something similar. Maybe in structure editor?

Bruce Shand
ST10 MP5 - Insight - Win10 - K4200

Re: Save draft file to desktop from Teamcenter

If you have the files opened - they should be in your local Cache.  therefore you can simply copy them from the cache to another folder location.

 

or, 

 

From Teamcenter you can simply download the named reference of the dataset. 

 

 

 

===================================================
Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7

Re: Save draft file to desktop from Teamcenter

Esteemed Contributor
Esteemed Contributor

@MattJohnson_PG, Ah, yes, I frequently forget about the cache.

Bruce Shand
ST10 MP5 - Insight - Win10 - K4200