Cancel
Showing results for 
Search instead for 
Did you mean: 

Save draft file to desktop from Teamcenter

Valued Contributor
Valued Contributor

I dont know if this can be done. My company uses Solid Edge with Teamcenter. If solid edge is connected to teamcenter, files are opened thru the server and teamcenter manages the file. If solid edge is not connceted to teamcenter files are opened from the PC disk drive. What I want to do, is to save a file I have opened from teamcenter to my local hard drive. I cannot see a way to do this either in Solid edge or in teamcenter.

3 REPLIES 3

Re: Save draft file to desktop from Teamcenter

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I don't have TC but I have used it and somewhere there is a "create unmanaged copy" function. Maybe not those words, which are from Insight, but something similar. Maybe in structure editor?

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Save draft file to desktop from Teamcenter

Gears Phenom Gears Phenom
Gears Phenom

If you have the files opened - they should be in your local Cache.  therefore you can simply copy them from the cache to another folder location.

 

or, 

 

From Teamcenter you can simply download the named reference of the dataset. 

 

 

 


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7

Re: Save draft file to desktop from Teamcenter

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Johnson_BigMatt, Ah, yes, I frequently forget about the cache.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200