Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Saving Radial Menu On Themes

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

How Can I Save The Theme On The Customize Radial Menu 

Set A New Theme Save As: Does Not Go To Save

 

Thank You

Crousie

2 REPLIES 2

Re: Saving Radial Menu On Themes

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Greg,

 

When you make any changes, the system will prompt you for a save to the current theme, or you can save as a different [existing, or user defined] one.

If this is not happening, do you have write access to the Solid Edge installation directory?

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Saving Radial Menu On Themes

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor
To Answer That Question About The Right Solid Edge Installation
I Do Not Think So