Cancel
Showing results for 
Search instead for 
Did you mean: 

Saving as type PDF option not showing

Experimenter
Experimenter

I'm pretty new to Solid Edge, but as I understand there should be an option to save the draft as a PDF file in the 'save as' menu, however this isn't showing up.

 

Anyone know a way to fix this?

6 REPLIES

Re: Saving as type PDF option not showing

MLombard
Retired

The PDF selection is in the drop down list in the save as dialog. You can also select Save As>Translated. Is this not happening?

 

SNAG-0044.png

Retired Community Manager for Solid Edge. This account is no longer active.

Re: Saving as type PDF option not showing

Experimenter
Experimenter

No Im not getting the option to save as a pdf

no pdf.jpg

Re: Saving as type PDF option not showing

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @brizvi,

 

Did you also notice you don't have the IGES option available either?.....I wonder if it's a glitch in the registry.

 

What version of SE [& maintenance patch - if appliccable] are you using here?

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Saving as type PDF option not showing

Siemens Phenom Siemens Phenom
Siemens Phenom

This is because you are running the free 2D product.  Free 2D does not have the capability to Save As to PDF.

Re: Saving as type PDF option not showing

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Good catch @uk_dave.

It would be helpful if more participants would include their workstation and software setup.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Re: Saving as type PDF option not showing

Siemens Phenom Siemens Phenom
Siemens Phenom

Save As Translated -- full blown Solid Edge:

screenshot.1459453946.png

 

Save As Translated -- free 2D:

screenshot.1459455428.png