Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Saving preferences and options in ST8

Master
Master

Just switched several machines to Windows 10 and ST8 this morning and trying to get them setup has been a challenge. Does any one know of a way to set one machine up as far as the startup screen , the list of standard templates, where you can go edit the list and have your user templates show up, and then save that to all the other machines?  I don't think this is under themes. I was hoping there was an eaiser way.

  Also we use the adminstrator options and I would have thought there was a way to disable FaceBook in it but I don't see a way.

 

Any suggestions?

 

Thanks,

Leonard

11 REPLIES 11

Re: Saving preferences and options in ST8

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Typically "options.xml".

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Saving preferences and options in ST8

Master
Master

Options.xml doesn't seem to hold the answers in this case. It's funny I can turn off the YouTube stuff from there but not the Facebook stuff.

 

Painful,

 

Leonard

Re: Saving preferences and options in ST8

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

As for options.xml I wasn't referring to the user assistance dock, I was referring to your question about templates and such.

Options.xml basically controls most of the settings in the file locations tab of the solid edge options.

If the user assistance docking window is your main concern then I misunderstood and I can't help. I never really care what's in it as we basically never use it.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Saving preferences and options in ST8

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hi Ilane,

for templates defined at Startup screen you shoud use the file "NewFileDefaultList.xml" located at folder %userprofile%\AppData\Roaming\Unigraphics Solutions\Solid Edge\Version 108\

If you copy the "NewFileDefaultList.xml" file to other machines, your templates shoud be already set at startup screen. However this is not "official" solution, but it should work.

 

Ota

Re: Saving preferences and options in ST8

Phenom
Phenom

Biggest gripe for me when setting up new users is having to manually set the Default Templates for every user using Solid Edge Options > Helpers > Default templates.

If you don't do this SE will use its own installed templates when converting files into SE instead of your own customised templates.

Been a while since I set up a new user but I think you also have to set the creation options list with Solid Edge Options > Helpers > Edit Creation Options.

This defines the the list of templates you get at the startup screen or File > New

HP Z420 16GB RAM
Quadro K4000
SE2019 MP5 on Windows 10 Pro 64.

Re: Saving preferences and options in ST8

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

Here's what i do for new machines. I go to the machine that's all set up. i go to the registry and export HKEY_CURRENT_USER\Sofware\Unigraphics Solutions to a network spot. I then go to the other computer and migrate the the file double click it. Now all the setting will be applied to that machine.

 

I did hear some where that in ST9 this should have this ability

Re: Saving preferences and options in ST8

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@beachcomber, Good point. This is yet another example of SE settings being scattered hither and yon.

@TDB, That's a neat trick if it's comprehensive and takes care of all default and custom settings including SE Options/file locations tab, helpers and such.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Saving preferences and options in ST8

Phenom
Phenom

Using the registry key is fine provided you don't apply it to a different user.

HP Z420 16GB RAM
Quadro K4000
SE2019 MP5 on Windows 10 Pro 64.

Re: Saving preferences and options in ST8

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Isn't that what @TDB was suggesting?

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200