Cancel
Showing results for 
Search instead for 
Did you mean: 

Saying good bye (for now)

Dear all, today is my last work day as a project engineer at EMCÉ Winches.

Per Monday I will start working for IHC SAS, they draw with Solid Works. I will keep my profile active due to the reason that in the future IHC SAS will start working with Solid Edge.

 

So for now, I say good bye to all of you.

 

Feel free to contact/link me via LinkedIN.

 


i-am-so-calm-as-it-is-my-last-day-at-the-office.png

 

 

 

-------
Daniël Schuiling
Solid Edge ST7
Teamcenter 10
9 REPLIES

Re: Saying good bye (for now)

Phenom
Phenom
Hi,

what is your email address Daniel - cannot add you via LinkedIn ?

Thanks.

Arek

Re: Saying good bye (for now)

Hi Arek,

 

I thought it was possible without email.

 

I will send you a message.

-------
Daniël Schuiling
Solid Edge ST7
Teamcenter 10

Re: Saying good bye (for now)

Gears Phenom Gears Phenom
Gears Phenom

Best of luck!  Thank you for your contributions to this community...   We hope its not too long before you come back to our beloved SE!

 

Till then...

===================================================
Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7

Re: Saying good bye (for now)

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Succes bij IHC Daniel

Re: Saying good bye (for now)

Legend
Legend

Hallo Daniel,

 

Ik wens je ontzettend veel succes en plezier bij IHC.

I wish you lots of success and fun at IHC.

 

Met vriendelijke groeten, 

Kind Regards,

 

 

Jan Bos

Solid Edge user since V3.5

 

 

 

Re: Saying good bye (for now)

Hi all,

 

it went faster than expected, but now I work in SE again.

 

Thank you all for the kind words.

-------
Daniël Schuiling
Solid Edge ST7
Teamcenter 10

Re: Saying good bye (for now)

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @DanielMCMLXXXII

 

 

 

a jovial welcome back to the group.

 

Does this mean, that they have swapt from SW2SE now?

 

This even is a better message, isn't it?

 

But again, welcome back and hope to read soon and very often from Your experiences.

 

regards
Wolfgang

Re: Saying good bye (for now)

Gears Phenom Gears Phenom
Gears Phenom

Kan je je e-mail ook sturen naar mij?

Bedankt!

Cgew9un

...........................................................................................................
Solid Edge 2019 & AutoCAD 2019 user

Re: Saying good bye (for now)

Hi Wolfgang,

At IHC SAS they still work with SW2014, but in the near future they are all going to work with SE and TC. It is the standard within IHC.

For me it is perfect, SW is nice but SE is like a old coat that I can wear again. Only now in ST7 instead of ST9, so some of the functions are missing.
-------
Daniël Schuiling
Solid Edge ST7
Teamcenter 10