Cancel
Showing results for 
Search instead for 
Did you mean: 

Scale tool, cannot find.

N/A
Newbie question, Where is the scale tool, I want to scale a circle, Searched help, and looked everywhere, can't find the button. Any help would be greatly apreaciated., Thank you.
2 REPLIES

Re: Scale tool, cannot find.

Siemens Phenom Siemens Phenom
Siemens Phenom
I will need more information as far as Scale, but I will assume that you just want to change the size of the circle. Click on the circle. You will see the circle's modify command ribbon. In this command ribbon is 'Diameter' and 'Radius'. Change the values to what you want. You can also specify the values at the time the circle is placed. Also, is you turn on 'Maintain Relationships', you can place a dimension on the circle and drive the diameter/radius by changing the dimension on the circle.

Regards,
Rick B.

Re: Scale tool, cannot find.

Esteemed Contributor
Esteemed Contributor
Scale command is located on the Sketching tab, Draw section, under the flyout menu displaying the Mirror button.


Ken

Production: ST10 MP5
Testing: SE 2019