Cancel
Showing results for 
Search instead for 
Did you mean: 

Scaling

Experimenter
Experimenter

Is there any way to scale down an assembly in Solid Edge v19?

5 REPLIES 5

Re: Scaling

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

One way that comes to mind is saving out the assembly as a parasolid X_T and importing back as a Part Copy with the desired scale.

 

Re: Scaling

Experimenter
Experimenter
Thank you!!

Re: Scaling

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Tushar wrote:

One way that comes to mind is saving out the assembly as a parasolid X_T and importing back as a Part Copy with the desired scale.

 


Why save it out as a parasolid? Just do part copy directly with that assembly.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Scaling

Gears Phenom Gears Phenom
Gears Phenom

Hi Edgers,

 

I have a DWG 2D drawing scaled to SCALE 1" = 25'-0"

 

Would you please tell me what Scale Factor Should I use to get 1:1?

 

thank you,

 

Arek

Re: Scaling

Genius
Genius

Hi @arekkul

 

My reasoning says it should be 300 (25' x 12").

585 ST10 Win 7