Cancel
Showing results for 
Search instead for 
Did you mean: 

Screen not updating when closing Explode Pathfinder

Valued Contributor
Valued Contributor

Hi

 

I have run into an annoying problem with ERA in ST9, when i close the "Explode Pathfinder" the screen doesn't update (see attached image). I have to tab out or switch to another window within SE and back again. It might not sound like a big deal but the reason for closing it is most often that i want to access parts and assemblies. And it's starting to become pretty annoying. How could one possibly fix this?

img01.png

3 REPLIES 3

Re: Screen not updating when closing Explode Pathfinder

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

First thing I would do is check to make sure your graphics driver is up to date. 

Re: Screen not updating when closing Explode Pathfinder

Valued Contributor
Valued Contributor

Thanks for taking the time to help. Turned out all it required to fix it was to restart SE. Sorry for the slow reply.

Re: Screen not updating when closing Explode Pathfinder

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
Hi @WJohnson,


just try to change the pathfinder style from transparent to solid and see wether this helps.

Another issue I personally prefer, is, to place all forms except the pathfinder to the right side of the screen and the pathfinder on the left, so that no form window is in conflict with the PF.

Just a try
regards
Wolfgang