Cancel
Showing results for 
Search instead for 
Did you mean: 

Screw mate

Creator
Creator

Hi, i'm searching something like the screw mate in SolidWorks, in which you can select a shaft and mate that to an hole and when you'll rotate the shaft in will advance like a screw in a threaded hole.

There is something similirar in SE or i have to make something like a path mate to an helical sketch?

 

1 REPLY 1
Highlighted

Re: Screw mate

Siemens Legend Siemens Legend
Siemens Legend

There are several ways to do this in SE but the simplest is to use the Gear relationship.

 

Run the command and select the Rotation-Linear option.

 

Hope this helps.

 

Thanks,

 

Art

 

Gear_Relationship.JPG