Cancel
Showing results for 
Search instead for 
Did you mean: 

Se 2D Draft St Tutorial Issues

N/A
I suppose this NG works both ways; users get some help on SE 2D and Siemens PLM in turn gets to learn what problems users are facing using their software. If this will help improve the software, I am posting the problems I am facing using the current tutorial version for ST2.
First of all, it would help if each step of the tutorial is numbered. That would make it easier for users to identify the step that users are referring to.
7 REPLIES

Re: Se 2D Draft St Tutorial Issues

N/A
This refers to the first tutorial on "Creating 2D Drawings with Solid Edge":
On Step 4; the page refers to a "Sketching tab" but there is no Sketching tab. I think an edit on this page is in order.

Re: Se 2D Draft St Tutorial Issues

N/A
In the "Draw a rectangle" step:
A reference is made to a Command Bar. In my mind, a bar is something that is longer than it is wide so this confused me a bit. I think a more appropriate description would be a Command Box.

Re: Se 2D Draft St Tutorial Issues

N/A
It has already been brought to my attention that the tutorials that were
delivered with Solid Edge 2D Drafting are the same as the ones that were
delivered with Solid Edge.
The command layouts are different between the two softwares.
This is why you are seeing a difference in command locations.
I am aware of this and have notified the appropriate individuals.
Regards,
Rick B.

Re: Se 2D Draft St Tutorial Issues

N/A
Does this mean it is pointless for me to comment further?

Re: Se 2D Draft St Tutorial Issues

N/A
There is no need to point out every instance where the tutorial does not
match the software.
Regards,
Rick B.

Re: Se 2D Draft St Tutorial Issues

N/A
I think anyone trying to learn the 2D will appreciate everything being listed Rick.
Thanks,
Dave

Re: Se 2D Draft St Tutorial Issues

N/A
I still want a user manual in PDF that I can print and have on hand while I'm working on projects. Maybe for ST3 we'll get lucky and have one.