Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Section Arrows

How can I set section arrows to different lengths as shown?

 

section_arrows.png

David McMahon
Solid Edge 2019
HP Z2 Mini, Windows 10
5 REPLIES 5

Re: Section Arrows

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Submit an ER to Siemens and wait...

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Section Arrows

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

You can't.  My guess is that Solid Edge is adhering to documentation standards such as ANSI, BSI, ISO, etc... 



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: Section Arrows

Builder
Builder

You sort-of can do it. You need to go into "Draw in View" and manually draw the lines as yo want them to show, then (or first) hide the real section view lines. It would be tedious, and could lead to mistakes later, but if you really need it to look like that...

Re: Section Arrows

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Yeah, you could, but you won't win any beauty contests. Smiley Happy

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Section Arrows

Thanks for the feedback. I read through ASME Y14.3, Multiview and Sectional View Drawings, and did not see anything stating that the arrow lengths need to be equal. I also checked the IHS Drawing Requirements Manual and didn't see anything in there. I know that other CAD packages such as Autodesk Inventor and Creo allow the section arrows to have different lengths which is convenient when trying to work around other drawing geometry or dimensions. I will submit an ER.

David McMahon
Solid Edge 2019
HP Z2 Mini, Windows 10