Cancel
Showing results for 
Search instead for 
Did you mean: 

Section not "Sectioning"

Not applicable

In the assembly I need to section a construction to expose a bolt inside for a technical drawing. There are two plates and a nut that the bolt is inserted through, yet the section option only cuts one of the plates OR the nut no matter what I do. I need it to cut through all the 4 parts to expose the bolt inside the plates and the nut...

There must be SOMETHING I'm missing, because it works just fine on the university lab computers, but it just won't work for me back home :/

3 REPLIES 3

Re: Section not "Sectioning"

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
So are you using the PMI section in the Assembly file to do this or are you creating a Section View in the Draft file to do this?


Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: Section not "Sectioning"

Not applicable
I am using the PMI Section option, and I have no idea why it doesn't work properly...

Re: Section not "Sectioning"

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
If using ST6, create a video and upload to YouTube and paste the link here. It will help with the diagnosis.
Sent from my Motorola Electrify using Tapatalk 2


Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com