Cancel
Showing results for 
Search instead for 
Did you mean: 

Servers

Experimenter
Experimenter

How do I connect to a local server. I appear to be connected to California which renders the software unuseable?

10 REPLIES 10

Betreff: Servers

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @RJD

 

 

render, server, California, local ?

 

Can You better explain this?

regards
Wolfgang

Betreff: Servers

Experimenter
Experimenter

Hi Wolfgang

 

Yeah, I downloaded the 45 day ST10 course. I am based in the UK but for some reason I am connected to the server in California which makes using the software slow bordering on unuseable. How can I resolve this problem?

Betreff: Servers

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@RJD  I don't know much about using the cloud hosted evaluation, but is there an option to download it?  If so, that's what I would suggest.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com
Highlighted

Betreff: Servers

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

HI @RJD

 

 

this makes me a little surprising.

 

I thought the 45 days trial version wil be downloaded (installation image) will be installed and YOu will recieve a license with an appropriate time stamp in it.

 

So after installing it correctly, I supposed that there is no  need for an online connection to use it.

 

Maybe this should be confirmed

 

 

regards
Wolfgang

Betreff: Servers

Siemens Phenom Siemens Phenom
Siemens Phenom

@hawcad FYI, we offer our 45-day trial in two version:

 

Either as the download with a standalone license which is what you are referring to

 

OR

 

As a streaming online option which I assume is what @RJD is referring to

 

2017-09-29 19_05_50-Solid Edge Download.png

 

 

Betreff: Servers

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @uk_dave

 

 

as I like to say:

 

"It's never to late for learning something new!"

 

I did not know that there is a streaming version too.

 

After let us know this, is this an option for standard SE licenses too?

So can one convert a e.g. floating or node locked license to such a streaming one?

 

regards
Wolfgang

Betreff: Servers

Siemens Phenom Siemens Phenom
Siemens Phenom

@hawcad  the streaming Solid Edge is currently only available for 45-day trials.  There is not a purchasable streaming Solid Edge option available at this time.

 

You should be able to sign up for a 45-day trial and give it a try if you're interested in "pushing the buttons".

Betreff: Servers

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @uk_dave

 

 

 

thanks for that info!

 

When I will find to have enough time fo rit I will give it a try!

 

 

regards
Wolfgang

Betreff: Servers

Experimenter
Experimenter

Evening Gentlemen

 

I have now tried both options (download and streaming). The streamed version is served by  a Californian server, which is useable but you lose the tutorial pane. So unless you memorise the lesson......

The download version is the one which is painfully slow but, you do get to keep the tutorial pane so you can read along as you learn.

Any suggestions?