Cancel
Showing results for 
Search instead for 
Did you mean: 

Setting Up Series Of K[holes

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

Good Evening

I Have This Short Video That Explains What I Am After. This Part Is A Di For A Pellet Mill. 

As Shown In The Background Is An Image Of A Die.I Would Like To Insert K[holes Though The Part With The Radius 120° Inside The Angle.

Any Thought On How This Could Be Accomplished.download (1).jpg6.jpg

ring-dies-.jpg

(view in My Videos)

1 REPLY

Re: Setting Up Series Of K[holes

Esteemed Contributor
Esteemed Contributor

Greg,

 

These "ring die's" would normally be created in the sheet metal environment, using a cylindrical construction in "Contour Flange".....see my attached ST7 example. [right click on the "Pattern" feature. and select "Unsuppress", to show the holes....only did this for a smaller file to upload]

 

ST7_PSM_Ordered_PerforatedBarrel_UnsuppressPattern.png

 

12-1.jpg   12-2.jpg

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP6] Classic [x2 seats]
Windows 10 - Quadro P2000