Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Setting decimal place precision on hole reference in dimension

Gears Phenom Gears Phenom
Gears Phenom

IIRC you can set precision of smart depths by using property text formatting...  

 

but without dbl-checking, I can not swear by it...  maybe custom callout but not smart depth???

 

It can be achieved however, I do know that.  maybe just not as cleanly as we'd like. 

 


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7
Highlighted

Re: Setting decimal place precision on hole reference in dimension

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Johnson_BigMatt

Hi @kjoiner

 

 

 

sorry for insisting and asking, but where do You want exactly which setting?

 

For a callout or for a dimension?

What is Your preferenced item?

 

 

regards
Wolfgang

Re: Setting decimal place precision on hole reference in dimension

Gears Phenom Gears Phenom
Gears Phenom

@hawcad I don't have a preference perse'  was just chiming in on the thread.   but...

 

since asked,  since we use hole call out to dim holes most of the time I would prefer as a hole callout enhancement.

 

I believe the ability is already there for Dimensions... 

 


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7

Re: Setting decimal place precision on hole reference in dimension

Gears Phenom Gears Phenom
Gears Phenom

@hawcad

 

I would like to be able to control the hole depth decimal place in the dimension tool.

 

Kyle

Kyle Joiner
IPA LLC
ST10 MP1

Re: Setting decimal place precision on hole reference in dimension

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Johnson_BigMatt

HI @kjoiner

 

 

OK I have got it.

But I think this is not working so far, even not with ST10!

regards
Wolfgang

Re: Setting decimal place precision on hole reference in dimension

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I prefer using smart dims for holes also. It's very odd that these precision codes like %{%TD/@2} work in callout smart depth but not in dims set as callouts with smart depth set identically.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200