Cancel
Showing results for 
Search instead for 
Did you mean: 

Setting

Genius
Genius

Hi Guys.

 

I have been updating our templates which has gone well.

 

Sometimes when we download a model (lets say a motor) some parts are not visible, this is down to surface and contruction settings.

 

Is there a way I can turn these set to on by default in my template?

I am using ST7.

 

Kind regards

 

Darren.

1 REPLY 1

Betreff: Setting

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Dazzie

 

 

if the question is going to "Is it possible to turn on surfaes in assemblies to be shown automatically?" then I think the answer will be no.

 

If it goes to "Surfaces in the part file are not shown as surfaces but only egdes are visible, then the answer is Yes.

You can change an option under the options - View Tab turning "Use Shading On Constructions" On!

 

 

20181218_1643.png

regards
Wolfgang