Cancel
Showing results for 
Search instead for 
Did you mean: 

Shared BOM settings

Builder
Builder

What is the best way to have my BOM table settings on a network drive so that multiple users can have access to it? Currently I have to setup my deptartments BOM settings on everyones computer indivually. 

2 REPLIES 2

Re: Shared BOM settings

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Put draftlist.txt on a server in a folder. Point to the folder in file locations in settings/options. It's probably now pointing to the template folder under c:\program files\solid edge\template.

That's about the most basic approach. It can get more involved. We share all the files under template\reports and also the materials and gage table and the holes excel files. And it's set up via options.xml which is edited via seadmin.exe. So all you have to do then is set everyone's file locations by changing the top line of the file locations dialog.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Shared BOM settings

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor