Cancel
Showing results for 
Search instead for 
Did you mean: 

Sharing Library

Experimenter
Experimenter

Hello all!

 

I am new to Solid edge 2D Draft. Since a couple of guys at the company are using it, I was wandering if we can share the library. What I mean is, if there is a possibility to share the library so all of us can see the drawings of all the others. Hope you understand what I mean.

 

Thank you in advance

Gojc

2 REPLIES 2

Re: Sharing Library

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

You need to set up a "shared folder".  If you have a network storage device/server, you can do it there.  If not, elect on of your PC's and create it there.  The other two PC's will then create a mapped drive to this shared folder.



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com

Re: Sharing Library

Experimenter
Experimenter

Thank you Grundey.