Cancel
Showing results for 
Search instead for 
Did you mean: 

Sheet Metal - Create une internal flange

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hello,

 

What is the best way to create a flange shown in the image attached?

There are any feature to do this in une single step?

 

Thank you,

 

Regards

Ricardo Ramos

 

 

4 REPLIES 4
Highlighted

Betreff: Sheet Metal - Create une internal flange

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @RicardoRamos

 

 

 

execpt of the "Offset" I do not understand, where it is, I would model it nearly exactly the same.

 

I can not see how the cutout is made, but I suppose this is a small slot feature (or here a symmetric offset)

As said, maybe I would use a slot, since it is less effort to get it.

 

But the rest would be the same

 

regards
Wolfgang

Re: Sheet Metal - Create une internal flange

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

You need a cutout feature and a bend feature to what you want. I suggest making a Feature Library from it and you can use anytime.

 

Here is a video:

 

BR, 

Imics
http://solidedgest.wordpress.com/

Betreff: Sheet Metal - Create une internal flange

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hi Wolfgang,

 

Tank you four your help,

I did offset to remove a clearance between flange and tab.

 

Regards,

 

Ricardo

Re: Sheet Metal - Create une internal flange

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hi Imics,

 

Your video is great.

I also think this is the best solution.

But if Solid Edge had a feature to do this it was great. We just need sketch the profile.

 

regards

Ricardo