Sheet Metal Gage

Valued Contributor
Valued Contributor

If we start a sheet metal part, we set our predefined "sheet metal gage" in the material table of the part.

Is it possible to display that predefined value on the draft of that part, so the construction people see which VE tu use to bend the plate?

PS: until now we don't use the flat patterns on drawings

8 REPLIES

Re: Sheet Metal Gage

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

"gage" is not currently exposed for use as property text...

 

BUT,  you can expose the material thickness variable and use that as property text as the best workaround currently.

Matt Johnson
Application Engineer
Ally PLM Solutions
matt.johnson@allyplm.com
http://allyplm.com/

Re: Sheet Metal Gage

Legend
Legend
You should be able to do this in ST6, its been working for me.
%{Gage|GP}
Using SE since V12, 2002

Re: Sheet Metal Gage

Valued Contributor
Valued Contributor

%{Gage|GP} does work, Thx

Great forum so far :-) 3 questions, 3 solutions

Re: Sheet Metal Gage

Creator
Creator

I am essentially a novice in solid edge and I'm a bit at a loss here. I am the only person in our company that consistently uses sheet metal, I am not sure what the question is here, I just pull a dimension off the metal thickness somewhere or put the thickness in the box we have for material specification.

Re: Sheet Metal Gage

Esteemed Contributor
Esteemed Contributor

Using Property Text in Draft and pulling such things as material and gauge from the attached model allows you to set up templates to automate the pulling and displaying of this data so you don't have to manually create a dimension or it lets you put it in the title block or in a note.


Thanks,
Ken

Production: ST9 MP10
Testing: ST10 MP3

Re: Sheet Metal Gage

Legend
Legend
Another advantage is that you can set up gages based on nominal dimensions or gage number. Also I set up plate thickness as PL1/4 etc. We in the US may be that last ones working this way but there are still a lot of us!
Using SE since V12, 2002

Re: Sheet Metal Gage

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hello together,

 

I was searching for this solution and i am very happy to find it here...

 

I have just one problem, I use an german Solid Edge there this %{Gage|GP} is not found....

 

If i change my language to english it works fine....

 

Has anyone an idea to get the information without changing the language?

 

Thanks in advance


lking wrote:
You should be able to do this in ST6, its been working for me.
%{Gage|GP}

 

Re: Sheet Metal Gage

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

I found the solution on my own....

 

english UI --> %{Gage|GP}

 

german UI --> %{Blechtafel|GP}