Cancel
Showing results for 
Search instead for 
Did you mean: 

Sheet metal Bead Command is shown unsuccessful what can i do ?

Experimenter
Experimenter

I have Problem in Sheet metal when i bend profile after i do the bead than operation unsuccesfull is seen kindly anybody tell me how it is happend?

1 REPLY 1

Betreff: Sheet metal Bead Command is shown unsuccessful what can i do ?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Rvpatel007

 

 

 

thee is a suppose I have and this could be due to after creating a bead in a sheet metal part You only can rebend it to the inner side of this bead.

Or otherwise round, the bead only can show to the outside of the bend, not to the inside.

 

20171106_0817.PNG

regards
Wolfgang