Cancel
Showing results for 
Search instead for 
Did you mean: 

Sheet metal bends

How I can ceate an animation for bending sheet to 90° ?

Someone can send me a sample file or video ?

Thanks 

8 REPLIES 8

Betreff: Sheet metal bends

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @RobertoGiussani

 

 

Try to define this PSM part as adjustable, with the bend angle as adj. variable.

Place it in an assembly and connect this variable to an ask variable.

And that one can drive a motor.

 

regards
Wolfgang

Re: Sheet metal bends

Genius
Genius

Hi friend, check this video may be of your help.

 

Regards.

 

 

Re: Sheet metal bends

Now all is clear ... thank you ...

Re: Sheet metal bends

Sorry but I return on this question ... I follow the same operation of the video but the created animation don't work.

The bend is simple at 90° and I wnat create animation from 179,99° to 90°.

Please help me again.screenshot.jpg

Re: Sheet metal bends

Genius
Genius

Hi friend, there is no problem for your worry, check this new video can be more helpful.

 

Regards.

Re: Sheet metal bends

OK work !!! I forgot to activate "NIVEL ACTIVE" ... and not "ASSEMBLY ACTIVE" THANK YOU VERY MUCH

Re: Sheet metal bends

Animation in SOLIDEDGE is OK but remain a little question ... I can't use thi type of animation in KEYSHOT 7 ... I need to find another solution ... Best regards and thanks again

Re: Sheet metal bends

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @RobertoGiussani

 

 

 

Yes this is true, Adjustable Parts are not supported in the KeyShot4Se license.

Maybe this would be possible in a greater Keyshot license, but this only could be answered by a Keyshot expert or partner.

Maybe You can ask this question in a Keyshot forum

 

 

regards
Wolfgang