Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Sheet metal cone (with flange)

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Ok, now it is clear to me...

 

I have thought about it, and see attached video

Re: Sheet metal cone (with flange)

Genius
Genius

Hello,

 

Sorry, my bad, now I will try to fix my mistake.

 

For making flang on a top of cone You can switch to part enviroment and make a revolwe (flatness is unavilable in this case) or use tool to wrapping shore in sheet metal enviroment (which is shown in the attached screenshot) but in this case you have limited choice of the shape of the bend.

SE ST9 + TC 10.1.7

Re: Sheet metal cone (with flange)

Phenom
Phenom

Easiest way is to do it as a part and just revolve the cross section - thats only one step.

The reason you can't add a flange around a curved edge is probably because that isn't a true bend - it relies on metal deformation.

Should still be possible though, and a good enhancement request.

 

@Wollverine - you can use the hem command with the Open and Bend Outside options to create the bend.

Then you can use a contour flange to create the flat.

Would need to set the angle of the hem according to the cone angle - so a bit of calculation there.

HP Z420 16GB RAM
Quadro K4000
SE2019 MP5 on Windows 10 Pro 64.
Highlighted

Re: Sheet metal cone (with flange)

Phenom
Phenom

Just realised contour flange will work if you include the curve of the bend.

The cone height would have to be adjusted accordingly, but you can do that by creating the full contour, then using that to position the sketches for the lofted flange.

HP Z420 16GB RAM
Quadro K4000
SE2019 MP5 on Windows 10 Pro 64.

Re: Sheet metal cone (with flange)

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @beachcomber

 

 

again one of the hidden secrets of SE.

 

Sketching the radius for that contour flange makes it working while let it create the bend radius by itself fails

 

 

regards
Wolfgang

Re: Sheet metal cone (with flange)

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

Here is a solution (similar to @beachcomber's):

 

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: Sheet metal cone (with flange)

Genius
Genius
Hey,

I try that when i wos serching solution for this topic and that didnt work for me corectly at that moment (sweep wos at 360 deg when profile wos opened, probably I had broken something) but i try again i works corecty now!

This is best solution
SE ST9 + TC 10.1.7