Cancel
Showing results for 
Search instead for 
Did you mean: 

Sheet metal dustbin

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hello Community,

 

I need some help,

I liked to do a dustbin like the photo but I have dificults to create the lateral slots.

 

2019-01-25 14_31_18-Window.jpg

 

I think I should do to make a pattern of the upper circles and the lower circles, and after that we joining the circles with a slot cut

I've tried create in Ordered and Synchronous, but in none of them did I get a good result.

 

2019-01-25 15_30_44-Window.jpg2019-01-25 15_30_17-Window.jpg

 

Attashed I send you the files do see the results.

Regards

Ricardo

7 REPLIES 7
Highlighted

Re: Sheet metal dustbin

Genius
Genius

Hi friend, does it refer to what is expressed in the image?

 

Regards.

 

 

KWLF_SHEET.jpgKWLF_SHEET_2.jpg

Re: Sheet metal dustbin

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hi Kanwulf,

 

Yes, that's exactly it.
Can you share the file?
Thank you

Ricardo

Re: Sheet metal dustbin

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
Hi there @RicardoRamos,

Wow, there's a trash bin shape, almost exactly the same that I made a model for, a time ago. As the nice work by @Kanwulf, it is not too challenging once you get the steps.

One thing though....if this was going to production, I would recommend placing the weld seem at the mid point of a slot....and likely, model it as two (front & rear) parts, if step folding using a press brake.
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Sheet metal dustbin

Genius
Genius

Hi Ricardo, of course, I hope it is of your help. Robot Happy

Re: Sheet metal dustbin

Genius
Genius

Thanks Sean. Smiley Very Happy

Re: Sheet metal dustbin

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hi Kanwulf

 

Thank you...

Re: Sheet metal dustbin

Gears Phenom Gears Phenom
Gears Phenom

Great job Guys! 

Imics
http://solidedgest.wordpress.com/