Cancel
Showing results for 
Search instead for 
Did you mean: 

Sheet metal flange issue

Builder
Builder

I need to remove a portion of a flange where it intersects another flange, please can someone advise on how to to this ? See attached sketch. thank you

9 REPLIES

Re: Sheet metal flange issue

Pioneer
Pioneer

Hi,

 

Open this flange as a sketch and change the contours to appropriate shape, or just unbend the flange and do simple cut off.

 

Regards,

 

Arek

Solid Edge ST8 MP10

Re: Sheet metal flange issue

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

In this case I suggest using contour flange command. Smiley Wink

 

Or use "Edit profile or Dynamic Editing" where you can modify angle and after this all use Close 3-Bend corners command! 

 

Here is a short video:

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: Sheet metal flange issue

Builder
Builder

Thank you for the video, I have tried this however it will not work, please see attached error message

Re: Sheet metal flange issue

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

@Imics

You have an answer for every problem.

You are the Guru !!

    

I am learning only through your examples. No help document can match this.  

Thanks a lot for a clean and informative video !!

   

Regards,

Tushar

 

Re: Sheet metal flange issue

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@agoodwin, you seem to have picked a face instead of just an edge or edges for the contour.

Bruce Shand
ST10 MP7 - Insight - Win10 - K4200

Re: Sheet metal flange issue

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Tushar, "You are the Guru !!"

I think Deity might be more appropriate.

Bruce Shand
ST10 MP7 - Insight - Win10 - K4200

Re: Sheet metal flange issue

Honored Contributor
Honored Contributor

Very nice.

Re: Sheet metal flange issue

Phenom
Phenom

Looks likie the base is possibly a PART not a shettmetal part? I'm not seeing a bend radius or a bend relief for the intersecting bends?

 

Lofted flanges wont work if you need the bend faces to be co planer and the loft edge is NOT perpendicular to the original bend line. see video for the differencees.  If faces need to be co planer I'd bend one flange then use loft, but check option to miter end cut. The proceed to add materila using tab.

 

-Craig

Re: Sheet metal flange issue

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hi

 if we need to close all the four side of this object in this way. Then what should We can do?

 

 

Regards

Vikram

ST9 MP3