Cancel
Showing results for 
Search instead for 
Did you mean: 

Sheet metal frame?

Honored Contributor
Honored Contributor

Is threre a way to have a sheet metal cross section be used as the section within the frame tool? When complete, I want to turn the frame parts into flat patterns.

2 REPLIES

Re: Sheet metal frame?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi Scott,

 

I don't believe so.....due to the way frame elements are derived, based on a single cross section profile, the relevant info for the sheet metal functions are not adhered to.

 

Not to say you couldn't convert the frame elements to sheet metal after saving them out.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP8] Classic [x3 seats]
Windows 10 - Quadro P2000
Testing: Solid Edge 2019

Re: Sheet metal frame?

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

Yes, Sean is right! There is no direct way, beacues sheet metal section is not supported.

 

Here is an example:

 

BR,

Imics
http://solidedgest.wordpress.com/