Cancel
Showing results for 
Search instead for 
Did you mean: 

Sheetmetal question

Dear SE users, I have a sheetmetal question.

I need to make a cable guiding gutter. I want it to have a slight angle so the cable can be lifted to the desired height. Now in the design I want to close the huge cap between 2 flanges that are also not aligned.

Any thoughts how to close this? See the attachment for the ST8 sheetmetal file.

-------
Daniël Schuiling
Solid Edge ST7
Teamcenter 10
8 REPLIES

Re: Sheetmetal question

Gears Phenom Gears Phenom
Gears Phenom

Wat wil je juist sluiten?

Kan je het eventueel snel krabbelen op een screenshot?

...........................................................................................................
Solid Edge 2019 & AutoCAD 2019 user

Re: Sheetmetal question

Hoi Joris, zie de afbeelding hieronder.

Hopelijk is het duidelijk.

20151217_100520[1].jpg

 

Wat ik wil is dat 2 flenzen verbonden zijn door middel van een extra part dat er precies tussen past. Echter moet het ook te produceren zijn.

-------
Daniël Schuiling
Solid Edge ST7
Teamcenter 10

Re: Sheetmetal question

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @DanielMCMLXXXII,

 

I extended tabs that initially looked OK, but adding material there will not allow it to flat pattern....are you OK with having seperate parts to weld in?

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Sheetmetal question

That is the reason I made the flanges shorter so they don't hit each other at the flat Pattern.

 

So yes, I already thought it should be made with an extra part. But how do I make such a part that it fits perfectly with two flanges that are not aligned and a height difference?

 

If you have a solution I would really like to know it Smiley Happy

-------
Daniël Schuiling
Solid Edge ST7
Teamcenter 10

Re: Sheetmetal question

And we will weld it together so it is no problem.

-------
Daniël Schuiling
Solid Edge ST7
Teamcenter 10

Re: Sheetmetal question

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@DanielMCMLXXXII,

 

OK...this is what I would do,....just a quick & dirty version for one side, so you can get the work flow I used. [see attached ST8 file]

I stayed in ordered mode, as per your original part.

 

Capture.PNG

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Sheetmetal question

Thank you @SeanCresswell

-------
Daniël Schuiling
Solid Edge ST7
Teamcenter 10

Re: Sheetmetal question

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Very welcome @DanielMCMLXXXII.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000