Cancel
Showing results for 
Search instead for 
Did you mean: 

Sheets PageUp and PageDown - Macro

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

I had asked this question sometime back in this forum and also saw a recent thread about using the PageDn and PageUp keys to cycle through sheets in Solid Edge Draft just as in Excel.

 

Download these two macros:

1. SheetNext.exe

2. SheetPrevious.exe

 

Extract the exe and image files to a single folder and attach them to two button anywhere on the ribbon in a lesser crowded area.

 

02.png

Tipp.png Read a tutorial to call macros from ribbon buttons with images.

 

Assign keyboard shortcuts Ctrl+PageUp and Ctrl+PageDown to the two ribbon buttons.

The above tutorial shows keyboard assignment too.

 

01.png

 

Note: Press the actual PageUp key in the customize dialog and not type 'P a g e  U p' - I did this silly thing  Robot Embarassed

Then forget about the buttons and start using the shortcuts Ctrl+PageUp and Ctrl+PageDn.

 

You will appreciate:

1. When the last working sheet is active, PageUp takes you to the first working sheet. It cycles through all working sheets continuously and does not stop when the last sheet is reached - unlike Excel !

Same with PageDn which cycles through sheets backwards - relentlessly.

 

So if you are at sheet 8 of 10 working sheets and want to go, to say, sheet 2, keep pressing PageUp to reach sheet 2 faster than pressing PageDown several times.

Same with PageDn.

  

Foot notes:

• Written to Work with Working sheets only - no pun intended !

• Not available in SW, Inventor, Creo and other such history-only programs.

  
~Tushar Suradkar

www.CADVertex.com

 

16 REPLIES 16

Re: How to Navigate sheets using PageUp and PageDown

Valued Contributor
Valued Contributor
Will this work in older versions of SE? Currently running ST3.

Erick

Re: How to Navigate sheets using PageUp and PageDown

Genius
Genius

Hi Tushar,

 

Just want to say thank you for your efforts made on this forum to make this available for the SE community.

It does work just fine ! (Like always)

Small things with great results Man Wink

Dirk Rutten

Solid Edge ST6 user !!!!

Re: Sheets PageUp and PageDown - Macro

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Brilliant as always @Tushar......and yet another of your creations, that deserves to exist as standard within "vanilla" Solid Edge!

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP6] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Highlighted

Re: Sheets PageUp and PageDown - Macro

Genius
Genius

Nice work

SE ST9 + TC 10.1.7

Re: Sheets PageUp and PageDown - Macro

Gears Phenom Gears Phenom
Gears Phenom

This is cool!

 

I'm inviting you for a beer in Cincinnati!

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: Sheets PageUp and PageDown - Macro

Gears Phenom Gears Phenom
Gears Phenom
Great macro Tushar !

Re: How to Navigate sheets using PageUp and PageDown

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

@esawyer wrote:
Will this work in older versions of SE? Currently running ST3.

Erick

Hi Erick:

  

I am on ST 6

Is it working for you ?

  

~Tushar

www.CADVertex.com

Re: How to Navigate sheets using PageUp and PageDown

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

@Xedu wrote:

Hi Tushar,

 

Just want to say thank you for your efforts made on this forum to make this available for the SE community.

It does work just fine ! (Like always)

Small things with great results Man Wink


Hi Dirk:

 

You are welcome.

Thank you for your words of appreciation.

 

~Tushar

Re: Sheets PageUp and PageDown - Macro

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

@SeanCresswell wrote:

Brilliant as always @Tushar......and yet another of your creations, that deserves to exist as standard within "vanilla" Solid Edge!


Thanks @SeanCresswell

May this wish of yours and mine come true.

 

~Tushar