Cancel
Showing results for 
Search instead for 
Did you mean: 

Short on Memory

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

Working in Assembly,

 

Within 20 to 45 min of opening in assy. the low memory comes. Why?

 

Thank You Greg

 

5 REPLIES

Re: Short on Memory

Hello Greg,

What version of Solid Edge and maintenance pack are you using?

Regards,
Theodore
Kind regards,
Theodore Turner

Re: Short on Memory

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor
I have Solid Edge ST6 Student Edition.
maintenance pack unknown.

Thank You
greg

Re: Short on Memory

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Greg,

 

The system memory [RAM] must be being consumed, by the assembly being displayed, plus any other applications running in the background, this includes Windows itself.

What does the assembly look like?....it may just be too detailed, with small faces...so if the graphics adaptor RAM is overwhelmed, it will draw from the system RAM....this case is even worse if it's a shared RAM [non-dedicated] type setup.

 

ALSO....the current build of Solid Edge Student Edition is ONLY in 32bit code, so is limited to [allocated] the amount of memory it can access [address].

 

What are your system specs? [CPU speed, RAM amount, Graphics adaptor type & RAM, HDD type & size]

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP7] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: Short on Memory

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

SeanCresswell wrote: 

ALSO....the current build of Solid Edge Student Edition is ONLY in 32bit code, so is limited to [allocated] the amount of memory it can access [address].


 

Further to this.....I believe ST7 [when it becomes available] is ONLY available in 64bit architecture. I can only summise that Student Edition will also follow this move.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP7] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: Short on Memory

Community Manager Community Manager
Community Manager

A better question is how much RAM do you have and what OS are you using? 

Dan Staples
Director, Solid Edge Product Development