Cancel
Showing results for 
Search instead for 
Did you mean: 

Show Exposed Variable In Drawing Table

I'm experimenting with displaying exposed variables in a drawing table but I can't it to work. I added the exposed variables to the table but the numeric values are not displaying. On a side note, if I create a callout using the exposed variable, it works. See attached files.

 

 

exposed_variable.jpg

David McMahon
Solid Edge 2019
HP Z2 Mini, Windows 10
2 REPLIES 2

Re: Show Exposed Variable In Drawing Table

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hi,

since the Variables are in the Top Assembly, you have to include it to the parts list.

PartListTopAsm.png

 

 

 

regards

JB
SE 2019, VS2017

Re: Show Exposed Variable In Drawing Table

Awesome, that fixed it!

David McMahon
Solid Edge 2019
HP Z2 Mini, Windows 10