Cancel
Showing results for 
Search instead for 
Did you mean: 

Show Image Within Part

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

I Went To Sketch Command To The Image Then Installed Into That Part... I Would Like To Know If There Is A Way Of Showing That Image Into The Assembly... I Do Not Want The View Override In The Assembly Command.

 

Thanks

Gregory Lee

5 REPLIES 5

Betreff: Show Image Within Part

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @PO_LC

 

 

 

can You describe more detailed what You want to do?

 

 

 

regards
Wolfgang

Betreff: Show Image Within Part

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

This Short Video Will Show You The Image That Is Embedded In The Part And The Assembly Part... And Also, The Glass See Through... I Do Not Remember Getting To Back To This Step. Any Thoughts 

 

Thanks

Gregory Lee

Betreff: Show Image Within Part

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @PO_LC

 

 

OK, I'm understanding now.

 

Simply use RMB on the part You want let to show the sketch pictures and turn on "Show sketch" (as shown in picture)

 

20161206_1946.PNG20161206_1948.PNG

 

This should You show the sketch from within the part.

 

 

regards
Wolfgang

Betreff: Show Image Within Part

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @PO_LC,

 

 

 

 

maybe You haven't used a sketch picture but a texture onto a certain surface.

But this should be visible anyway

 

 

regards
Wolfgang

Betreff: Show Image Within Part

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

You may need to check the "show textures" in the view overrides dialogue:

 

Show Textures.JPG

 

Kyle

Kyle Joiner
IPA LLC
ST10 MP1