Cancel
Showing results for 
Search instead for 
Did you mean: 

Show Intersection lines on drg?

Valued Contributor
Valued Contributor

The dimension shown below dimensions to the intersection of the inside bends. the problem with that is it isnt clear where the dimension is going to. Is there a way to show intersection lines as dashed lines or something similar.
Capture.PNG

Regards,

MagRiz
(ST9 User Est 01.18)
18 REPLIES 18

Betreff: Show Intersection lines on drg?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @MagRiz

 

 

 

the visual info when selecting the dimension is not what Your are looking for, isn't it?

 

20180420_125602.png

regards
Wolfgang

Betreff: Show Intersection lines on drg?

Valued Contributor
Valued Contributor

@hawcad

 

Hi, no not that. its after the dimension has been placed  - i want to see those line on the draft view. 

Regards,

MagRiz
(ST9 User Est 01.18)

Betreff: Show Intersection lines on drg?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @MagRiz

 

 

so OK, than there are two option I see immedeately:

 

Either change the ettings for Your dimensions to not have any gap for Projection Lines

 

20180420_1317.png

 

 

or to add small circle in view add those intersection points.

I use thme for dimensioning too:

 

20180420_1321.png

regards
Wolfgang

Betreff: Show Intersection lines on drg?

Phenom
Phenom

Hi @MagRiz,

 

you could do it with the Centerline

Centerline.jpg

 

 

 

 

 

 

 

 

 

Yasser

Betreff: Show Intersection lines on drg?

Valued Contributor
Valued Contributor

@YD thats not right as its not the intersection you're dim'ing to.

Regards,

MagRiz
(ST9 User Est 01.18)

Betreff: Show Intersection lines on drg?

Valued Contributor
Valued Contributor

@hawcad thanks, but thats not quite what im after 

 

see this video, https://www.youtube.com/watch?v=dSoYdZRIWP8 

 

SW has virtual sharps which is what im used to.

 

Regards,

MagRiz
(ST9 User Est 01.18)

Betreff: Show Intersection lines on drg?

Phenom
Phenom

Betreff: Show Intersection lines on drg?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @MagRiz

 

 

so no there are no dimension options or setting to get them by itself.

 

BTW:

if You always compare SE with SW You will not get happy it all.

What does not mean that we can not try to improve SE functionality.

And virtual point extensions of course would be one good enhancement.

 

And regarding to another post "Smart DIm is not Smart", I just have seen in the video, that in SW You also have/can/must press CTRL, SHIFT etc., to define which option You want.

So there is no big difference to smart dimension with Shift or A pressed?

 

regards
Wolfgang

Betreff: Show Intersection lines on drg?

Valued Contributor
Valued Contributor

Wolfgang,

 

The two circles that you showed...  are they dimension properties or are they points that you stuck in manually?

 

Matt