Cancel
Showing results for 
Search instead for 
Did you mean: 

Show base body feature in draft.

Gears Phenom Gears Phenom
Gears Phenom

I used a body feature from our supplier and did some cut and drill.

Nuw I make a draft, but for the supplier it would be a big help if I could show the original body feature around my part.

Can I do this, other than making an assembly of both and make the base part a reference part?

...........................................................................................................
Solid Edge 2019 & AutoCAD 2019 user
2 REPLIES

Betreff: Show base body feature in draft.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Joris

 

 

 

You can do this from one and the same part file too.

 

Just use multibody functionallity.

 

Start with the imported body (supplier body) from Your supplier, create a second body, do a copy (surface) from the base body and create Your operations in it.

 

Creating a draft You will find both boodies in the draft display list, from where You can change the supplier body to be shown as e.g. reference

 

20180228_1512.PNG

 

 

 

Here is the part itself too:

 

20180228_1514.PNG

regards
Wolfgang

Betreff: Show base body feature in draft.

Gears Phenom Gears Phenom
Gears Phenom

Thanks, I'll keep this in mind for a next project!

...........................................................................................................
Solid Edge 2019 & AutoCAD 2019 user