Cancel
Showing results for 
Search instead for 
Did you mean: 

Show hidden components

Valued Contributor
Valued Contributor

If I hide components in my assy, is there a way to show them collectively but isolated. So other non-hidden components are hidden, temporarly.

 

Similar to the Show hidden components on SolidWorks

Regards,

MagRiz
(ST9 User Est 01.18)
23 REPLIES 23

Betreff: Show hidden components

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @MagRiz

 

 

 

AFAIK there is no equivilant function to that You mentioned for SW.

 

But give the "Toggle Disply" function a try.

This IMHO is the nearest function to what You request.

 

20180130_1715.PNG

 

 

I normally have this as a Keyboard Shortcut (Alt-T) in use

regards
Wolfgang
Highlighted

Re: Show hidden components

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

I am not sure if there is a better way to do this, but you can create a query that searches for all hidden components whose author is not "-" (arbitrarily picked since you must use some property and this should return all hidden components).  If you double click the query it will run and select all hidden compoenents in the assembly.  You can then right-click in space and choose Isolate to enter the Isolate view of just those hidden components. You can then Restore whenever you are finished to go back to the original view.  If you choose Dismiss option, then the current view will remain.

Betreff: Show hidden components

Valued Contributor
Valued Contributor

ahh, this is a really good feature. But if it isolated too that would be better that way i can easily find the hidden parts in large assys

Regards,

MagRiz
(ST9 User Est 01.18)

Re: Show hidden components

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @ChrisMerz

 

 

 

this is a great method to achieve a fast switch to the hidden components and vice versa!

 

Great Smiley Happy

 

 

regards
Wolfgang

Re: Show hidden components

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

See this short video and if it matches your requirement, download the free app from the page mentioned below the video:

 

 

http://www.cadvertex.com/download.htm

See the second macro from bottom or simply search the page.

  

Tushar

www.SurfAndCode.IN

 

Re: Show hidden components

Gears Phenom Gears Phenom
Gears Phenom

Hi @Tushar

 

I have applied this macro into St10 and unfortunatelly it isnt working.

I am getting strange SE behaviour like blinking the screen etc.

 

regards,

Arek

Re: Show hidden components

Valued Contributor
Valued Contributor

This works for me @Tushar but how do I add the macro to the ribbon?

i went on to customise the ribbon but i cant find macros in that long list

Regards,

MagRiz
(ST9 User Est 01.18)

Re: Show hidden components

Valued Contributor
Valued Contributor

Re: Show hidden components

Valued Contributor
Valued Contributor

thanks got it working now.

 

I've only been using SE for 6 days and i'm trying to get it to match as much as SW as i can Smiley Very Happy

 

Regards,

MagRiz
(ST9 User Est 01.18)