Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Show hidden components

Valued Contributor
Valued Contributor
I can understand, I tried this too with SW, while I used it Smiley Happy But I'm sure SE has a better user experience. I missing a few minor feature from SW, like "Show hidden components". But SE has a way much better stability and predictability.
So go ahead, you will have fun!
SE2019 MP3

Re: Show hidden components

Valued Contributor
Valued Contributor

you're right about stability no crashes yet. but SW has a better UI and quicker way of doing things.

Regards,

MagRiz
(ST9 User Est 01.18)

Re: Show hidden components

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

@MagRiz wrote:

This works for me @Tushar but how do I add the macro to the ribbon?

i went on to customise the ribbon but i cant find macros in that long list


See this blog page. Just under the free apps area are 4 tutorials to add macros to various UI places in Solid Edge:

http://www.surfandcode.in/2014/01/index-of-all-tutorials-on-this-solid.html

 

AppsArea.png

Re: Show hidden components

Genius
Genius

Hi

I have added this macro, but I appear to have the same problem as Arek. When I click the macor button, the PathFinder flickers several times and then I get the message pop-up asking if I want to report the problem to Microsoft. I am using ST9 MP13 on Windows 7. Any ideas?

Thanks.

585 ST10 Win 7

Re: Show hidden components

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Sorry to hear that the macro is flickering the Pathfinder

I tested it originally in ST6 and yesterday again in ST10 before posting but found no problems.

This could be due to the assembly being very small - one of those from the training folder having no more than 10-12 components.

Are you checking the macro in a large assembly ?

Re: Show hidden components

Gears Phenom Gears Phenom
Gears Phenom

Hi @Tushar,

 

yes, the assembly contains 1371 parts.

 

regards,

Arek

Re: Show hidden components

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Hi @arekkul

  

I will test the macro on a larger assembly, with components close to what you have mentioned.

 

   

Regards,

Tushar

 

Highlighted

Re: Show hidden components

Genius
Genius

Hi Tushar

 

The assembly I have tried has 565 components with 6 levels and 49 subassemblies.

 

Thanks.

585 ST10 Win 7

Re: Show hidden components

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Hi @585

  

I am able to verify the problem with an assembly of just 150 parts with 4 levels.

In my case the Pathfinder flickers for some time but it does not run into an error.

It does the job.

   

I will revisit the code again and check if its performance could be improved.

There's in fact nothing much that the code does beyond checking which components are hidden/shown and toggling their display state. I believe it has more to do with the display performance and the supporting hardware, especially the graphics card.

 

Thanks.

 

Tushar

 

Re: Show hidden components

Genius
Genius

Hi Tushar

My system is a Dell Precision T3610 with Xeon 4 Core 3.7GHz. Graphics card is a Quadro K2000 with 2GB.

Many thanks for your assistance.

585 ST10 Win 7