Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Show hidden components

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Hi @585

 

Mine is a DELL PRECISION M6800 with  16 GM RAM, i7 2.8 GHz CPU with nVidia Quadro K3100M graphics card.

So no relief seems to be in sight anytime soon Smiley Sad until I bump into some sort of scoop to rev up the performance of the little macro.

 

I will consult the heavyweights of programming - Jason Newell and Martin Bernhard later this week.

Till then, let's keep fingers crossed.

 

Tushar

 

Re: Show hidden components

Gears Phenom Gears Phenom
Gears Phenom

Hi @Tushar

 

My data:

Proc.png

Graphics : AMD FirePro W7100

 

cheers,

Arek

Highlighted

Re: Show hidden components

Genius
Genius

Thanks for your help Tushar. It is not a big problem for me if you can't get a solution, it is a nice to have feature.

585 ST10 Win 7

Re: Show hidden components

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

@MagRiz wrote:

thanks got it working now.

 


@MagRiz

 

Kindly mark all relevant messages as 'Accepted Solutions'.

This is necessary because the discussion has already spread over 4 pages and in future someone visiting this discussion should be able to find the solution directly.

Also people who contributed get credit and recognition. This is a popular forum practice.

Thanks.