Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Show the icon Hide last layer (Ctrl+Q) in the ribbon

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hi everybody,

 

Into an assembly file, searching for the Hide last layer (Ctrl+Q command), it doesn't appear in the ribbon, moreover opening the costumize options, it appears to be already placed in the ribbon.

 

Thanks,

 

RicardS

 

Solid Edge ST10 MP8

1 REPLY 1

Re: Show the icon Hide last layer (Ctrl+Q) in the ribbon

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Hi @RicardS

 

It is on the View tab, Show group on the ribbon

But you have to be in the "Edit mode" for a part in the assembly to see it.

 

CtrlQHPL.png

 

If you "Close and Return" from the Edit mode, the button will not be seen since it is not applicable in the default assembly mode, but the shortcut Ctrl+Q will remain assigned for this command and will be listed in the Customize dialog list for assigned shortcuts.

  

Hope this helps.

 

Tushar

www.SurfAndCode.IN