Cancel
Showing results for 
Search instead for 
Did you mean: 

Showing the dimensions of copied parts in parts lists.

Experimenter
Experimenter

We are setting up our Parts Lists to show part dimensions that are driven from part files.  All is working smoothly except in the case of parts generated as copies of original parts (i.e mirrored copy).  With copied parts, no dimensions show their variables tables thus preventing the creation of links that will drive dimensions of the affected parts in the parts list.  Is there a solution to this problem?  If possible, we want to avoid overiding cells in our parts lists and manually entering values. 

5 REPLIES 5

Betreff: Showing the dimensions of copied parts in parts lists.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @dogpatch75

 

 

 

You can use my MainDImension macro therefore.

 

I think this can help to get it.

 

 

See post 

https://community.plm.automation.siemens.com/t5/Solid-Edge-Forum/Listing-Dimensons-of-parts-in-part-...

 

 

but I will attach the macro again, so that You can use the current version of it.

And of course this is a free tool to use!

 

 

Take a look into the 2 XML files.

Within them You can define nearly anything You want to have

 

Explanantion is there in English too!

 

Hope it helps

 

regards
Wolfgang

Betreff: Showing the dimensions of copied parts in parts lists.

Experimenter
Experimenter
MainDim after unpacking will not open on my Windows 7 system.

Betreff: Showing the dimensions of copied parts in parts lists.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @dogpatch75

 

 

do You have a 3D document open?

 

Is there any error message?

 

 

regards
Wolfgang

Betreff: Showing the dimensions of copied parts in parts lists.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

...

 

 

HI @dogpatch75

 

 

which Solid Edge Versionis installed?

 

Maybe if You have ST10 then tehre is the 32bit API missing.

 

See other post and install View&Markup too.

This will install 32bit again

 

regards
Wolfgang
Highlighted

Re: Showing the dimensions of copied parts in parts lists.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

We use mirrored parts a lot and what happens is the exposed variable in the original part becomes a custom text property in the mirrored part. Let's say it's called "length". So we delete the custom property length, then add a PMI dim and expose it as "length". Then it will show up in the parts list.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200