Cancel
Showing results for 
Search instead for 
Did you mean: 

Showing thread on Section View draft.

Valued Contributor
Valued Contributor

I have a revolved part where i have added a thread to a cylindrical surface. 

 

when ive sectioned that part on my drawing i cant see the thread. 

 

i have gone into properties of the view (and parent view) and selected - Show threads in Section Only section views. but this has made no difference 

Regards,

MagRiz
(ST9 User Est 01.18)
17 REPLIES 17

Betreff: Showing thread on Section View draft.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @MagRiz 

 

 

 

can You upload the part and the draft?

regards
Wolfgang

Betreff: Showing thread on Section View draft.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @MagRiz 

 

 

 

I remember, that there was a bug in SE2019 without MP, but this already is fixed since months, and You signature shows that You are using ST9

 

There is a single situation where a thread is not shown in a draft section and that is, when the section does not go exactly through the center.

 

This always is a good indicator to check the section line position and to always use a relation to fix it there.

 

 

regards
Wolfgang

Betreff: Showing thread on Section View draft.

Valued Contributor
Valued Contributor

Hi @hawcad 

 

unfortunately i cant upload the draft file, but what i might do is create a new part/ drawing and try it on there and send that if it doesnt work.

 

im confident the section goes through the centre

Regards,

MagRiz
(ST9 User Est 01.18)

Betreff: Showing thread on Section View draft.

Valued Contributor
Valued Contributor

@hawcad 

 

See attached file 

Regards,

MagRiz
(ST9 User Est 01.18)

Betreff: Showing thread on Section View draft.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @MagRiz 

 

 

OK, immedeatelly seen.

This can not work.

 

You have a 12mm core hole and put a M12 thread on it!

 

For inner threads I allways recommend to use a hole feature.

You even can create the counter bore hole with thread and chamfers in one step

 

See images:

 

20190214_1118.png20190214_1123.png20190214_1128.png

regards
Wolfgang

Betreff: Showing thread on Section View draft.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @MagRiz 

 

 

 

the only point I would like to claim here is, that IMHo Solid Edge must not allow to create such a feature at all!

This must be prevented by the system and may not depend on a users choice.

So from that point of view, it is not You failure, it more is a weak functionality and control mechanism of SE.

 

regards
Wolfgang

Betreff: Showing thread on Section View draft.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @MagRiz 

 

 

and another information I hav eto give to YOu is how to "repair" it for Your existing part.

 

I would reduce the inner diamter of that revolution to e.g. 8mm and would add a thread hole afterwards.

 

See images:

 

20190214_1134.png20190214_1135.png20190214_1136.png

regards
Wolfgang

Betreff: Showing thread on Section View draft.

Valued Contributor
Valued Contributor

thanks, i cant see the images, but i get what you mean - i need to model the tapping drill size (10.2 for M12) then put the thread on after. 

 

Regards,

MagRiz
(ST9 User Est 01.18)

Betreff: Showing thread on Section View draft.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Can you guys see the images that @hawcad included?

 

All I see are triangles.

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200