Cancel
Showing results for 
Search instead for 
Did you mean: 

Silent installs and femapapi.e​xe RM CC4 Network failing to install.

Creator
Creator

Hi Folks

 

I've setup my deployment for SolidEdge ST7 added my MST file with licence details and this works fine when running the deployment via cmd prompt. When I create a RM CC4 package the install starts fine but gets stuck at some point near the end.

 

Event 1000

 

Faulting application path c:\program files\Solid Edge ST7\Simulation\x64\femapapi.exe

 

same error on X64 or x32 stations.

 

Looks like when the error happens the interactive services detection pops up.  I got the same error with ST6 downloaded ST7 and same. 

 

Anyone with a CC4 network manage to get this installed?