Cancel
Showing results for 
Search instead for 
Did you mean: 

Simplified / Design Frames Possible?

Pioneer
Pioneer

Can anyone explain,

Is there possibility to make holes & cutouts in  frame designed component, like square & round pipe?

 

Regards,

 

Somnath

4 REPLIES 4

Re: Simplified / Design Frames Possible?

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

Yes, you have to use Assembly features!

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: Simplified / Design Frames Possible?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @Somnath_Pore,

 

Yes, using assembly features.

 

2018-08-07.png

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Simplified / Design Frames Possible?

Pioneer
Pioneer

I tried, but not happening.

What is the reason?

 

Regards,

Somnath

 

Re: Simplified / Design Frames Possible?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Somnath_Pore,

 

Assembly features are constructed in an "ordered mode" fashion, so you need to define each step [plane, profile, extent] correctly, and also, what part[s] are to be included [normally the extent takes care of selection, but you can over-ride it] in the feature. These are normally trouble free to contruct, so is a little puzzling.

 

Can you record your screen, to include all steps, right up until it fails?.....that would help identify what might be causing the issue.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000