Cancel
Showing results for 
Search instead for 
Did you mean: 

Simplifying Assemblies- removing sub assemblies

Experimenter
Experimenter

I am running ST8, I have an assembly that is made of multiple sub assemblies that I want to make into an assembly of components.  I want to basically keep all the components of the sub assemblies in place and just no longer have them lock in the sub assembly so if items are removed  from the main assembly it does not effect the former sub assembly.  

 

This is needed when I convert the large assembly into a STP file to send to a customer.  The file is way too big when the assembly is left whole so I remove the inner components to leave the visible outer parts.

5 REPLIES

Re: Simplifying Assemblies- removing sub assemblies

Honored Contributor
Honored Contributor

You will want to dig into the Transfer command (Assembly/modify)

I don't do much exporting. Is suppress sufficient to prevent export?

The Pack and Go commands are also worth a look.   Never mind that's ST9

 

When It comes to file sizes of exports, it's the complex imported parts that take up the space. Re-modeling a few complex often used pieces to a simpler model really helps the export size.

 

I had a single imported pump that was costing me 5 megs per copy. After some re-modeling w/ sufficient detail, it now takes up 0.5 megs each copy. Huge swing when the goal is to email the files.

Re: Simplifying Assemblies- removing sub assemblies

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@RickS_  Is there a question?

Bruce Shand
ST10 MP7 - Insight - Win10 - K4200

Re: Simplifying Assemblies- removing sub assemblies

Experimenter
Experimenter

Thank you.  Although the Transfer was not what I was wanting the Disperse command did what I needed.  Just needed to know where to look.

 

 

Re: Simplifying Assemblies- removing sub assemblies

Honored Contributor
Honored Contributor

No worries. That is often my problem too. I can navigate the room, but where the hell is the door to get into the room is the common problem.

Re: Simplifying Assemblies- removing sub assemblies

Phenom
Phenom

When you do the convert you can opt to convert visible parts only (in the Options settings)

Just hide the parts you don't want to convert.

To make future conversions easier it might be an idea to create simplified sub-assemblies, or create view configurations in the sub-assembly model with internal parts hidden. Call it "External Only" or something easlily identifiable.

Then in your main assembly select the sub-assembly and click the configurations drop-down. You should see your sub-assembly config listed there. Select it and the config will be applied to that sub-assembly.

HP Z420 16GB RAM
Quadro K4000
ST10 MP6 on Windows 10 Pro 64.