Cancel
Showing results for 
Search instead for 
Did you mean: 

Simulation Express

Experimenter
Experimenter

Good day.

 

I have a problem with simulation express in ST8.

 

The simulation just does not show any result. It seems like its getting cancelled automatically after a few seconds of starting the analysis. Also the system is not showing any errors for this.

 

Just to be clear, there is no issue with the part modelling as i have run the same part on another system and there it worked perfectly.

 

Are there any settings to look for to resolve this ? Any help would be great.

 

Regards,

Puskar

9 REPLIES 9

Re: Simulation Express

Phenom
Phenom

No file/log, no solution Smiley Wink

 

Harri

Re: Simulation Express

Experimenter
Experimenter

Hi harri,

 

You mean the part file, right ?

 

I have tried simulating as simple parts as a L-shape bracket. It's not working only on my system and i can't figure out why.

 

 

 

Re: Simulation Express

Phenom
Phenom

@Puskar_P , yep. However this will be impossible to debug without a little more info. Can you post the file or a short video showing the steps you took when setting up the simulation? 

Re: Simulation Express

Experimenter
Experimenter

@hjoy  I have attached the file. I follwed the below steps:

1. selected the part

2. Material

3. force (chose face for the force)

4. constraint- fixed one side of the cylinder

5. analyze

I have attached the screen shot till the analysis runs. After this it come back to normal without any error and results.

 

Hope it helps.

 

Re: Simulation Express

Phenom
Phenom

@Puskar_P , the file appears to be missing..

Re: Simulation Express

Experimenter
Experimenter

 @hjoy  ohh sorry. may be only one file uploads at a time. Attached again.

Re: Simulation Express

Phenom
Phenom

Seems the simulation itself is ok, runs on SE2019. Let's hope someone with ST8 will chime in.

 

(view in My Videos)

 

Harri

Re: Simulation Express

Experimenter
Experimenter

@hjoythanks for trying. The file is working on ST8 installed on other system as well. I think it may be some installation issue or glitch with the software.

Re: Simulation Express

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Puskar_P 

 

 

and what happens if another user logs into Your computer?

Same story means a computer issue, different means user issue!

 

regards
Wolfgang