Cancel
Showing results for 
Search instead for 
Did you mean: 

Simulation of frame based on curves

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hi,

I would like to run simulation in Solid Edge of frame which is odd - not only linear but curved beams. I created 3D curve in part, somehow transformed into sketch. In assembly I can make a frame on it, but within simulation beam curves are not generated on this 3D curve.

I want to be sure of limitation that beam curves can be generated only on lines or arcs, but not on 3D curves.

Or is it possible to run simulation of 3D curved beam?

I run such analysis in NX and it works.

Juraj

3 REPLIES

Re: Simulation of frame based on curves

Siemens Phenom Siemens Phenom
Siemens Phenom

Juraj, 

a Simulation study on curved Frames is possible.

 

If not possible on your model maybe contact your local support.

 

Good luck /Ulf

 

 

Siemens EMEA GTAC Support

Re: Simulation of frame based on curves

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

Simulation doesn't support curves (splines) to analyzing.

 

BR,

 

Imics
http://solidedgest.wordpress.com/

Re: Simulation of frame based on curves

Siemens Phenom Siemens Phenom
Siemens Phenom

Yes, if based on b-spline Curves that is true. Lines & Arcs was what I used.

Siemens EMEA GTAC Support